public interface PostScenarioManager extends Remote
PostScenarioBuilder
. nxopen.CAE#postScenarioManager
. Modifier and Type | Method and Description |
---|---|
boolean |
checkScenarioDataSourceCompatible(PostScenarioParameters scenarioParameters)
Checks if the scenario and the data source set in the
PostScenarioParameters are compatible. |
boolean |
checkValidDataSource(PostScenarioParameters scenarioParameters)
Checks if the data source set in
PostScenarioParameters is valid. |
PostScenarioBuilder |
createPostScenarioBuilderFromParameters(PostScenarioParameters scenarioParameters)
Creates a transient object
PostScenarioBuilder that is
responsible for creating a post scenario object. |
PostScenarioBuilder |
createPostScenarioBuilderFromViewport(int viewportIndex)
Creates a builder for the Scenario retrieved from a Visualized Scenario from a certain viewport.
|
PostScenarioParameters |
newPostScenarioParameters()
Creates a transient object
PostScenarioParameters that
contains the settings required to create a post scenario. |
PostScenarioDescriptorCollection |
postScenarioDescriptors()
Contains a
PostScenarioDescriptorCollection . |
PostScenarioDescriptorCollection postScenarioDescriptors() throws RemoteException
RemoteException
PostScenarioParameters newPostScenarioParameters() throws NXException, RemoteException
PostScenarioParameters
that
contains the settings required to create a post scenario.
The object should be destroyed after the post scenario is created.
NXException
RemoteException
boolean checkValidDataSource(PostScenarioParameters scenarioParameters) throws NXException, RemoteException
PostScenarioParameters
is valid.
scenarioParameters
- NXException
RemoteException
boolean checkScenarioDataSourceCompatible(PostScenarioParameters scenarioParameters) throws NXException, RemoteException
PostScenarioParameters
are compatible.
scenarioParameters
- NXException
RemoteException
PostScenarioBuilder createPostScenarioBuilderFromParameters(PostScenarioParameters scenarioParameters) throws NXException, RemoteException
PostScenarioBuilder
that is
responsible for creating a post scenario object.
scenarioParameters
- NXException
RemoteException
PostScenarioBuilder createPostScenarioBuilderFromViewport(int viewportIndex) throws NXException, RemoteException
viewportIndex
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.