public static class PostAnnotationBuilder.Type extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ENTITY |
static int |
_MAX |
static int |
_MIN |
static int |
_USERLOC |
static PostAnnotationBuilder.Type |
ENTITY |
static PostAnnotationBuilder.Type |
MAX |
static PostAnnotationBuilder.Type |
MIN |
static PostAnnotationBuilder.Type |
USERLOC |
Modifier and Type | Method and Description |
---|---|
static PostAnnotationBuilder.Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostAnnotationBuilder.Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostAnnotationBuilder.Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final PostAnnotationBuilder.Type ENTITY
public static final PostAnnotationBuilder.Type MIN
public static final PostAnnotationBuilder.Type MAX
public static final PostAnnotationBuilder.Type USERLOC
public static final int _ENTITY
public static final int _MIN
public static final int _MAX
public static final int _USERLOC
public static PostAnnotationBuilder.Type valueOf(int value)
public static PostAnnotationBuilder.Type valueOf(String name)
public static PostAnnotationBuilder.Type[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.