public static class Post.Legend extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COLORBAR_ONLY |
static int |
_DETAILED |
static int |
_HEADER_ONLY |
static Post.Legend |
COLORBAR_ONLY |
static Post.Legend |
DETAILED |
static Post.Legend |
HEADER_ONLY |
Modifier and Type | Method and Description |
---|---|
static Post.Legend |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Legend |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Legend[] |
values()
Returns an array that contains the values for this enum.
|
public static final Post.Legend DETAILED
public static final Post.Legend COLORBAR_ONLY
public static final Post.Legend HEADER_ONLY
public static final int _DETAILED
public static final int _COLORBAR_ONLY
public static final int _HEADER_ONLY
public static Post.Legend valueOf(int value)
public static Post.Legend valueOf(String name)
public static Post.Legend[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.