public static class Post.GroupVisibility extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HIDE |
static int |
_SHOW |
static int |
_SHOW_ONLY |
static Post.GroupVisibility |
HIDE |
static Post.GroupVisibility |
SHOW |
static Post.GroupVisibility |
SHOW_ONLY |
Modifier and Type | Method and Description |
---|---|
static Post.GroupVisibility |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.GroupVisibility |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.GroupVisibility[] |
values()
Returns an array that contains the values for this enum.
|
public static final Post.GroupVisibility SHOW_ONLY
public static final Post.GroupVisibility SHOW
public static final Post.GroupVisibility HIDE
public static final int _SHOW_ONLY
public static final int _SHOW
public static final int _HIDE
public static Post.GroupVisibility valueOf(int value)
public static Post.GroupVisibility valueOf(String name)
public static Post.GroupVisibility[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.