public static class Post.Format extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTO |
static int |
_FIXED_POINT |
static int |
_SCIENTIFIC |
static Post.Format |
AUTO |
static Post.Format |
FIXED_POINT |
static Post.Format |
SCIENTIFIC |
Modifier and Type | Method and Description |
---|---|
static Post.Format |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Format |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Format[] |
values()
Returns an array that contains the values for this enum.
|
public static final Post.Format AUTO
public static final Post.Format FIXED_POINT
public static final Post.Format SCIENTIFIC
public static final int _AUTO
public static final int _FIXED_POINT
public static final int _SCIENTIFIC
public static Post.Format valueOf(int value)
public static Post.Format valueOf(String name)
public static Post.Format[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.