public static class Post.BandStyle extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEFAULT |
static int |
_LINE |
static int |
_VAL_INLINE |
static Post.BandStyle |
DEFAULT |
static Post.BandStyle |
LINE |
static Post.BandStyle |
VAL_INLINE |
Modifier and Type | Method and Description |
---|---|
static Post.BandStyle |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.BandStyle |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.BandStyle[] |
values()
Returns an array that contains the values for this enum.
|
public static final Post.BandStyle DEFAULT
public static final Post.BandStyle LINE
public static final Post.BandStyle VAL_INLINE
public static final int _DEFAULT
public static final int _LINE
public static final int _VAL_INLINE
public static Post.BandStyle valueOf(int value)
public static Post.BandStyle valueOf(String name)
public static Post.BandStyle[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.