public static class Post.AnimationControl extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BACK |
static int |
_DELAY |
static int |
_FULL_CYCLE |
static int |
_NEXT |
static int |
_PAUSE |
static int |
_PLAY |
static int |
_SET_FRAME |
static int |
_STOP |
static int |
_STREAMLINE |
static Post.AnimationControl |
BACK |
static Post.AnimationControl |
DELAY |
static Post.AnimationControl |
FULL_CYCLE |
static Post.AnimationControl |
NEXT |
static Post.AnimationControl |
PAUSE |
static Post.AnimationControl |
PLAY |
static Post.AnimationControl |
SET_FRAME |
static Post.AnimationControl |
STOP |
static Post.AnimationControl |
STREAMLINE |
Modifier and Type | Method and Description |
---|---|
static Post.AnimationControl |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.AnimationControl |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.AnimationControl[] |
values()
Returns an array that contains the values for this enum.
|
public static final Post.AnimationControl BACK
public static final Post.AnimationControl NEXT
public static final Post.AnimationControl PLAY
public static final Post.AnimationControl PAUSE
public static final Post.AnimationControl STOP
public static final Post.AnimationControl SET_FRAME
public static final Post.AnimationControl FULL_CYCLE
public static final Post.AnimationControl DELAY
public static final Post.AnimationControl STREAMLINE
public static final int _BACK
public static final int _NEXT
public static final int _PLAY
public static final int _PAUSE
public static final int _STOP
public static final int _SET_FRAME
public static final int _FULL_CYCLE
public static final int _DELAY
public static final int _STREAMLINE
public static Post.AnimationControl valueOf(int value)
public static Post.AnimationControl valueOf(String name)
public static Post.AnimationControl[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.