public interface PolygonGeometryManager extends Remote
PolygonGeometryManager
GeometryRecipeCollection
class to create a recipe. Modifier and Type | Interface and Description |
---|---|
static class |
PolygonGeometryManager.PolygonBodyResolutionType
Entity type
|
Modifier and Type | Method and Description |
---|---|
GeometryRecipeCollection |
caeGeometryRecipes()
Returns the geometry recipes belonging to the FEM.
|
PolygonGeometryManager.PolygonBodyResolutionType |
getPolygonBodyResolutionOnFemBodies()
Gets the tesselation on polygon bodies that were created from CAD bodies.
|
void |
setPolygonBodyResolutionOnFemBodies(PolygonGeometryManager.PolygonBodyResolutionType resType)
Sets the tesselation on polygon bodies that were created from CAD bodies.
|
CAEBody[] |
setPolygonBodyResolutionWithRecreate(PolygonGeometryManager.PolygonBodyResolutionType resolutionType,
CAEBody[] inPolygonBodies)
Set Resolution for polygon body with recreate body only
License requirements: nx_masterfem ("Finite Element Modeling") . |
CAEBody[] |
setPolygonBodyResolutionWithRecreateAndUpdate(PolygonGeometryManager.PolygonBodyResolutionType resolutionType,
CAEBody[] inPolygonBodies)
Set Resolution for polygon body with recreate body and update only
License requirements: nx_masterfem ("Finite Element Modeling") . |
GeometryRecipeCollection caeGeometryRecipes() throws RemoteException
RemoteException
void setPolygonBodyResolutionOnFemBodies(PolygonGeometryManager.PolygonBodyResolutionType resType) throws NXException, RemoteException
resType
- Tesselation on all polygon bodiesNXException
RemoteException
PolygonGeometryManager.PolygonBodyResolutionType getPolygonBodyResolutionOnFemBodies() throws NXException, RemoteException
NXException
RemoteException
CAEBody[] setPolygonBodyResolutionWithRecreate(PolygonGeometryManager.PolygonBodyResolutionType resolutionType, CAEBody[] inPolygonBodies) throws NXException, RemoteException
resolutionType
- inPolygonBodies
- NXException
RemoteException
CAEBody[] setPolygonBodyResolutionWithRecreateAndUpdate(PolygonGeometryManager.PolygonBodyResolutionType resolutionType, CAEBody[] inPolygonBodies) throws NXException, RemoteException
resolutionType
- inPolygonBodies
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.