public static class ModelDisplayBuilder.NodeDisplayModeType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXPLICIT
Nodes are explicitly shown and hidden via the Show/Hide commands.
|
static int |
_IMPLICIT
Nodes are implicitly shown according to the following rules.
|
static ModelDisplayBuilder.NodeDisplayModeType |
EXPLICIT
Nodes are explicitly shown and hidden via the Show/Hide commands.
|
static ModelDisplayBuilder.NodeDisplayModeType |
IMPLICIT
Nodes are implicitly shown according to the following rules.
|
Modifier and Type | Method and Description |
---|---|
static ModelDisplayBuilder.NodeDisplayModeType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ModelDisplayBuilder.NodeDisplayModeType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ModelDisplayBuilder.NodeDisplayModeType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ModelDisplayBuilder.NodeDisplayModeType IMPLICIT
public static final ModelDisplayBuilder.NodeDisplayModeType EXPLICIT
public static final int _IMPLICIT
public static final int _EXPLICIT
public static ModelDisplayBuilder.NodeDisplayModeType valueOf(int value)
public static ModelDisplayBuilder.NodeDisplayModeType valueOf(String name)
public static ModelDisplayBuilder.NodeDisplayModeType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.