public static class LaminateDrapingDataBuilder.DrapingDirectionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CSYS
Define draping direction using a coordinate system
|
static int |
_VECTORS
Define draping direction using vector(s)
|
static LaminateDrapingDataBuilder.DrapingDirectionType |
CSYS
Define draping direction using a coordinate system
|
static LaminateDrapingDataBuilder.DrapingDirectionType |
VECTORS
Define draping direction using vector(s)
|
Modifier and Type | Method and Description |
---|---|
static LaminateDrapingDataBuilder.DrapingDirectionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LaminateDrapingDataBuilder.DrapingDirectionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LaminateDrapingDataBuilder.DrapingDirectionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final LaminateDrapingDataBuilder.DrapingDirectionType VECTORS
public static final LaminateDrapingDataBuilder.DrapingDirectionType CSYS
public static final int _VECTORS
public static final int _CSYS
public static LaminateDrapingDataBuilder.DrapingDirectionType valueOf(int value)
public static LaminateDrapingDataBuilder.DrapingDirectionType valueOf(String name)
public static LaminateDrapingDataBuilder.DrapingDirectionType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.