public static class ElementConnectivityBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALL_ELEMENTS_ATTACHED_TO_NODE
Modify connectivities of all attached elements to nodes.
|
static int |
_SINGLE_ELEMENT
Modify connectivity of selected element.
|
static ElementConnectivityBuilder.Types |
ALL_ELEMENTS_ATTACHED_TO_NODE
Modify connectivities of all attached elements to nodes.
|
static ElementConnectivityBuilder.Types |
SINGLE_ELEMENT
Modify connectivity of selected element.
|
Modifier and Type | Method and Description |
---|---|
static ElementConnectivityBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementConnectivityBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementConnectivityBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final ElementConnectivityBuilder.Types SINGLE_ELEMENT
public static final ElementConnectivityBuilder.Types ALL_ELEMENTS_ATTACHED_TO_NODE
public static final int _SINGLE_ELEMENT
public static final int _ALL_ELEMENTS_ATTACHED_TO_NODE
public static ElementConnectivityBuilder.Types valueOf(int value)
public static ElementConnectivityBuilder.Types valueOf(String name)
public static ElementConnectivityBuilder.Types[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.