public static class DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAXIMUM_PRINCIPAL
Maximum Principal
|
static int |
_MAXIMUM_SHEAR
Maximum Shear
|
static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum |
MAXIMUM_PRINCIPAL
Maximum Principal
|
static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum |
MAXIMUM_SHEAR
Maximum Shear
|
Modifier and Type | Method and Description |
---|---|
static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum MAXIMUM_SHEAR
public static final DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum MAXIMUM_PRINCIPAL
public static final int _MAXIMUM_SHEAR
public static final int _MAXIMUM_PRINCIPAL
public static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum valueOf(int value)
public static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum valueOf(String name)
public static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.