public static class DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BWI |
static int |
_SMITH_WATSON_TOPPER |
static int |
_STRAIN_LIFE_MAXIMUM_PRINCIPAL |
static int |
_STRAIN_LIFE_MAXIMUM_SHEAR |
static int |
_STRESS_LIFE |
static int |
_TWI |
static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum |
BWI |
static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum |
SMITH_WATSON_TOPPER |
static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum |
STRAIN_LIFE_MAXIMUM_PRINCIPAL |
static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum |
STRAIN_LIFE_MAXIMUM_SHEAR |
static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum |
STRESS_LIFE |
static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum |
TWI |
Modifier and Type | Method and Description |
---|---|
static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum SMITH_WATSON_TOPPER
public static final DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum STRAIN_LIFE_MAXIMUM_PRINCIPAL
public static final DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum STRAIN_LIFE_MAXIMUM_SHEAR
public static final DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum STRESS_LIFE
public static final DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum BWI
public static final DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum TWI
public static final int _SMITH_WATSON_TOPPER
public static final int _STRAIN_LIFE_MAXIMUM_PRINCIPAL
public static final int _STRAIN_LIFE_MAXIMUM_SHEAR
public static final int _STRESS_LIFE
public static final int _BWI
public static final int _TWI
public static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum valueOf(int value)
public static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum valueOf(String name)
public static DurabilityDamageEvaluationBuilder.FatigueLifeCriterionEnum[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.