public static class CorrelAlignmentBuilder.ScalingChoice extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FROM_SECOND_AXIS
Computed from the lenght of the second axis
|
static int |
_SPECIFY
User specified scaling factor
|
static CorrelAlignmentBuilder.ScalingChoice |
FROM_SECOND_AXIS
Computed from the lenght of the second axis
|
static CorrelAlignmentBuilder.ScalingChoice |
SPECIFY
User specified scaling factor
|
Modifier and Type | Method and Description |
---|---|
static CorrelAlignmentBuilder.ScalingChoice |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CorrelAlignmentBuilder.ScalingChoice |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CorrelAlignmentBuilder.ScalingChoice[] |
values()
Returns an array that contains the values for this enum.
|
public static final CorrelAlignmentBuilder.ScalingChoice FROM_SECOND_AXIS
public static final CorrelAlignmentBuilder.ScalingChoice SPECIFY
public static final int _FROM_SECOND_AXIS
public static final int _SPECIFY
public static CorrelAlignmentBuilder.ScalingChoice valueOf(int value)
public static CorrelAlignmentBuilder.ScalingChoice valueOf(String name)
public static CorrelAlignmentBuilder.ScalingChoice[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.