public static class CfdContactPreventionConstraintBuilder.LocalSubdivisions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FIVE |
static int |
_FOUR |
static int |
_ONE |
static int |
_THREE |
static int |
_TWO |
static int |
_ZERO |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
FIVE |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
FOUR |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
ONE |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
THREE |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
TWO |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
ZERO |
Modifier and Type | Method and Description |
---|---|
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CfdContactPreventionConstraintBuilder.LocalSubdivisions[] |
values()
Returns an array that contains the values for this enum.
|
public static final CfdContactPreventionConstraintBuilder.LocalSubdivisions ZERO
public static final CfdContactPreventionConstraintBuilder.LocalSubdivisions ONE
public static final CfdContactPreventionConstraintBuilder.LocalSubdivisions TWO
public static final CfdContactPreventionConstraintBuilder.LocalSubdivisions THREE
public static final CfdContactPreventionConstraintBuilder.LocalSubdivisions FOUR
public static final CfdContactPreventionConstraintBuilder.LocalSubdivisions FIVE
public static final int _ZERO
public static final int _ONE
public static final int _TWO
public static final int _THREE
public static final int _FOUR
public static final int _FIVE
public static CfdContactPreventionConstraintBuilder.LocalSubdivisions valueOf(int value)
public static CfdContactPreventionConstraintBuilder.LocalSubdivisions valueOf(String name)
public static CfdContactPreventionConstraintBuilder.LocalSubdivisions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.