public class CaeSetObjectSubType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ELEMENT_EDGE
sub type is element edge
|
static int |
_ELEMENT_FACE
sub type is element face
|
static int |
_NONE
sub type is the same as the type of the object
|
static int |
_PART
sub type is part, used for Gravity Loads
|
static CaeSetObjectSubType |
ELEMENT_EDGE
sub type is element edge
|
static CaeSetObjectSubType |
ELEMENT_FACE
sub type is element face
|
static CaeSetObjectSubType |
NONE
sub type is the same as the type of the object
|
static CaeSetObjectSubType |
PART
sub type is part, used for Gravity Loads
|
Modifier and Type | Method and Description |
---|---|
static CaeSetObjectSubType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CaeSetObjectSubType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CaeSetObjectSubType[] |
values()
Returns an array that contains the values for this enum.
|
public static final CaeSetObjectSubType NONE
public static final CaeSetObjectSubType ELEMENT_FACE
public static final CaeSetObjectSubType ELEMENT_EDGE
public static final CaeSetObjectSubType PART
public static final int _NONE
public static final int _ELEMENT_FACE
public static final int _ELEMENT_EDGE
public static final int _PART
public static CaeSetObjectSubType valueOf(int value)
public static CaeSetObjectSubType valueOf(String name)
public static CaeSetObjectSubType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.