public interface CAEConnectionCollection extends TaggedObjectCollection
BaseFEModel
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
CAEConnectionBuilder |
createConnectionBuilder(CAEConnection connection)
Creates a builder for Connection Command
License requirements: nx_masterfem ("Finite Element Modeling") . |
CAEWeldConnectionBuilder |
createWeldConnectionBuilder(CAEWeldConnection weldconnection)
Creates a builder for WeldConnection Command
License requirements: nx_masterfem ("Finite Element Modeling") . |
CAEConnection |
findObject(String journalIdentifier)
Finds the
CAEConnection with the given identifier as recorded in a journal. |
_find_next, iterator
CAEConnection findObject(String journalIdentifier) throws NXException, RemoteException
CAEConnection
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Connection nameNXException
RemoteException
CAEConnectionBuilder createConnectionBuilder(CAEConnection connection) throws NXException, RemoteException
connection
- CAEConnection
to be edited,
if null then create a new oneNXException
RemoteException
CAEWeldConnectionBuilder createWeldConnectionBuilder(CAEWeldConnection weldconnection) throws NXException, RemoteException
weldconnection
- WeldConnection Recipe to be edited, if null then create a new oneNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.