public static class CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NODE_TO_NODE
Create elements between nodes on source and target edges.
|
static int |
_RBE2RBE3TO_ELEMENT_EDGE
Create RBE2 between source node and projected node, and RBE3 between projected node and target edge nodes.
|
static int |
_RBE2RBE3TO_ELEMENT_FACE
Create RBE2 bewteen source node and projected node, and RBE3 between projected node and target face nodes.
|
static CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum |
NODE_TO_NODE
Create elements between nodes on source and target edges.
|
static CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum |
RBE2RBE3TO_ELEMENT_EDGE
Create RBE2 between source node and projected node, and RBE3 between projected node and target edge nodes.
|
static CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum |
RBE2RBE3TO_ELEMENT_FACE
Create RBE2 bewteen source node and projected node, and RBE3 between projected node and target face nodes.
|
Modifier and Type | Method and Description |
---|---|
static CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum NODE_TO_NODE
public static final CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum RBE2RBE3TO_ELEMENT_EDGE
public static final CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum RBE2RBE3TO_ELEMENT_FACE
public static final int _NODE_TO_NODE
public static final int _RBE2RBE3TO_ELEMENT_EDGE
public static final int _RBE2RBE3TO_ELEMENT_FACE
public static CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum valueOf(int value)
public static CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum valueOf(String name)
public static CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.