public static class BeamSectionOffsetOptions.Method extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LANGUAGE_SPECIFIC
The offset coordindate system is defined in language-specific way.
|
static int |
_NEUTRAL
The offset coordindate system is defined in neutral way
|
static BeamSectionOffsetOptions.Method |
LANGUAGE_SPECIFIC
The offset coordindate system is defined in language-specific way.
|
static BeamSectionOffsetOptions.Method |
NEUTRAL
The offset coordindate system is defined in neutral way
|
Modifier and Type | Method and Description |
---|---|
static BeamSectionOffsetOptions.Method |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BeamSectionOffsetOptions.Method |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BeamSectionOffsetOptions.Method[] |
values()
Returns an array that contains the values for this enum.
|
public static final BeamSectionOffsetOptions.Method NEUTRAL
public static final BeamSectionOffsetOptions.Method LANGUAGE_SPECIFIC
public static final int _NEUTRAL
public static final int _LANGUAGE_SPECIFIC
public static BeamSectionOffsetOptions.Method valueOf(int value)
public static BeamSectionOffsetOptions.Method valueOf(String name)
public static BeamSectionOffsetOptions.Method[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.