public interface AutoPairs extends NXObject
Modifier and Type | Interface and Description |
---|---|
static class |
AutoPairs.CreateFacePairsData
This class holds the data returned from
createFacePairs() |
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
AutoPairs.CreateFacePairsData |
createFacePairs()
Create face pairs whose distance is less than the distance tolerance stored
in the recipe.
|
CAEBody[] |
getBodies()
Get the list of
CAEBody
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX5.0.0 |
CAEFace[] |
getFaces()
Get the list
CAEFace
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX5.0.0 |
PropertyTable |
propertyTable()
Returns the property table associated with the auto pairs object.
|
void |
setBodies(CAEBody[] faces)
Set the list of
CAEBody
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX5.0.0 |
void |
setFaces(CAEFace[] faces)
Set the list of
CAEFace
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX5.0.0 |
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
void setFaces(CAEFace[] faces) throws NXException, RemoteException
CAEFace
faces
- Selected facesNXException
RemoteException
CAEFace[] getFaces() throws NXException, RemoteException
CAEFace
NXException
RemoteException
void setBodies(CAEBody[] faces) throws NXException, RemoteException
CAEBody
faces
- BodiesNXException
RemoteException
CAEBody[] getBodies() throws NXException, RemoteException
CAEBody
NXException
RemoteException
AutoPairs.CreateFacePairsData createFacePairs() throws NXException, RemoteException
CAEFace
NXException
RemoteException
PropertyTable propertyTable() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.