public static class AfuMathOperation.TimeToSrsResponseType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ABSOLUTE_MAX
Absolute Maximum
|
static int |
_NEGATIVE_MAX
Negative Maximum
|
static int |
_POSITIVE_MAX
Positive Maximum
|
static AfuMathOperation.TimeToSrsResponseType |
ABSOLUTE_MAX
Absolute Maximum
|
static AfuMathOperation.TimeToSrsResponseType |
NEGATIVE_MAX
Negative Maximum
|
static AfuMathOperation.TimeToSrsResponseType |
POSITIVE_MAX
Positive Maximum
|
Modifier and Type | Method and Description |
---|---|
static AfuMathOperation.TimeToSrsResponseType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AfuMathOperation.TimeToSrsResponseType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AfuMathOperation.TimeToSrsResponseType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AfuMathOperation.TimeToSrsResponseType POSITIVE_MAX
public static final AfuMathOperation.TimeToSrsResponseType NEGATIVE_MAX
public static final AfuMathOperation.TimeToSrsResponseType ABSOLUTE_MAX
public static final int _POSITIVE_MAX
public static final int _NEGATIVE_MAX
public static final int _ABSOLUTE_MAX
public static AfuMathOperation.TimeToSrsResponseType valueOf(int value)
public static AfuMathOperation.TimeToSrsResponseType valueOf(String name)
public static AfuMathOperation.TimeToSrsResponseType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.