public interface AfuMathFastRMSInfo extends TransientObject
Modifier and Type | Interface and Description |
---|---|
static class |
AfuMathFastRMSInfo.Data
This class holds the data returned from
getData() |
Modifier and Type | Method and Description |
---|---|
AfuMathFastRMSInfo.Data |
getData()
Get the Fast RMS Parameter Information
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setData(int numberOfPoints,
int order,
int relativeOrder,
int useHighpassFilter,
double cutoffFraction,
int addSidelobes,
double slope,
int interpolationMethod)
Set the Fast RMS Parameter Information
License requirements: nx_ftk ("NX Advanced Graphing") . |
_value, dispose, printTestData, printTestData
void setData(int numberOfPoints, int order, int relativeOrder, int useHighpassFilter, double cutoffFraction, int addSidelobes, double slope, int interpolationMethod) throws NXException, RemoteException
numberOfPoints
- Set the Fast RMS PSD Fit number of pointsorder
- the orderrelativeOrder
- the relative orderuseHighpassFilter
- the use highpass filter optioncutoffFraction
- the filter frequency cutoff fractionaddSidelobes
- the add sidelobes optionslope
- the side lobes slope valueinterpolationMethod
- the interpolation methodNXException
RemoteException
AfuMathFastRMSInfo.Data getData() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.