public static class Tree.NodeInsertOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALWAYS_FIRST
Node is placed first in the hierarchy in which it is inserted.
|
static int |
_ALWAYS_LAST
Node is placed last in the hierarchy in which it is inserted.
|
static int |
_FIRST
Node is placed first in the hierarchy in which it is inserted.
|
static int |
_LAST
Node is placed last in the hierarchy in which it is inserted.
|
static int |
_SORT
Node is sorted according to display text and placed accordingly in the hierarchy in which it is inserted
|
static Tree.NodeInsertOption |
ALWAYS_FIRST
Node is placed first in the hierarchy in which it is inserted.
|
static Tree.NodeInsertOption |
ALWAYS_LAST
Node is placed last in the hierarchy in which it is inserted.
|
static Tree.NodeInsertOption |
FIRST
Node is placed first in the hierarchy in which it is inserted.
|
static Tree.NodeInsertOption |
LAST
Node is placed last in the hierarchy in which it is inserted.
|
static Tree.NodeInsertOption |
SORT
Node is sorted according to display text and placed accordingly in the hierarchy in which it is inserted
|
Modifier and Type | Method and Description |
---|---|
static Tree.NodeInsertOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Tree.NodeInsertOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Tree.NodeInsertOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final Tree.NodeInsertOption FIRST
public static final Tree.NodeInsertOption LAST
public static final Tree.NodeInsertOption SORT
public static final Tree.NodeInsertOption ALWAYS_FIRST
BlockStyler.Tree.NodeInsertOption#FIRST
, except that it
remains first after a column sort. If there is more than one node beneath a single parent
with this option then they will be sorted relative to each other.public static final Tree.NodeInsertOption ALWAYS_LAST
BlockStyler.Tree.NodeInsertOption#LAST
, except that it
remains last after a column sort. If there is more than one node beneath a single parent
with this option then they will be sorted relative to each other.public static final int _FIRST
public static final int _LAST
public static final int _SORT
public static final int _ALWAYS_FIRST
BlockStyler.Tree.NodeInsertOption#FIRST
, except that it
remains first after a column sort. If there is more than one node beneath a single parent
with this option then they will be sorted relative to each other.public static final int _ALWAYS_LAST
BlockStyler.Tree.NodeInsertOption#LAST
, except that it
remains last after a column sort. If there is more than one node beneath a single parent
with this option then they will be sorted relative to each other.public static Tree.NodeInsertOption valueOf(int value)
public static Tree.NodeInsertOption valueOf(String name)
public static Tree.NodeInsertOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.