public static class CreateNewComponentBuilder.ComponentLayerOptionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AS_SPECIFIED
Set the layer option type to as specified
|
static int |
_ORIGINAL
Set the layer option type to original
|
static int |
_WORK
Set the layer option type to work
|
static CreateNewComponentBuilder.ComponentLayerOptionType |
AS_SPECIFIED
Set the layer option type to as specified
|
static CreateNewComponentBuilder.ComponentLayerOptionType |
ORIGINAL
Set the layer option type to original
|
static CreateNewComponentBuilder.ComponentLayerOptionType |
WORK
Set the layer option type to work
|
Modifier and Type | Method and Description |
---|---|
static CreateNewComponentBuilder.ComponentLayerOptionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CreateNewComponentBuilder.ComponentLayerOptionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CreateNewComponentBuilder.ComponentLayerOptionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final CreateNewComponentBuilder.ComponentLayerOptionType ORIGINAL
public static final CreateNewComponentBuilder.ComponentLayerOptionType WORK
public static final CreateNewComponentBuilder.ComponentLayerOptionType AS_SPECIFIED
public static final int _ORIGINAL
public static final int _WORK
public static final int _AS_SPECIFIED
public static CreateNewComponentBuilder.ComponentLayerOptionType valueOf(int value)
public static CreateNewComponentBuilder.ComponentLayerOptionType valueOf(String name)
public static CreateNewComponentBuilder.ComponentLayerOptionType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.