public static class ComponentAssembly.SubstitutionMode extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALL
An associative substitution is performed on all components that
represent the same prototype part.
|
static int |
_NON_ASSOCIATIVE
The old component is deleted, and the new one is added
|
static int |
_SINGLE_COMPONENT
An associative substitution is performed.
|
static ComponentAssembly.SubstitutionMode |
ALL
An associative substitution is performed on all components that
represent the same prototype part.
|
static ComponentAssembly.SubstitutionMode |
NON_ASSOCIATIVE
The old component is deleted, and the new one is added
|
static ComponentAssembly.SubstitutionMode |
SINGLE_COMPONENT
An associative substitution is performed.
|
Modifier and Type | Method and Description |
---|---|
static ComponentAssembly.SubstitutionMode |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ComponentAssembly.SubstitutionMode |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ComponentAssembly.SubstitutionMode[] |
values()
Returns an array that contains the values for this enum.
|
public static final ComponentAssembly.SubstitutionMode NON_ASSOCIATIVE
public static final ComponentAssembly.SubstitutionMode SINGLE_COMPONENT
public static final ComponentAssembly.SubstitutionMode ALL
public static final int _NON_ASSOCIATIVE
public static final int _SINGLE_COMPONENT
public static final int _ALL
public static ComponentAssembly.SubstitutionMode valueOf(int value)
public static ComponentAssembly.SubstitutionMode valueOf(String name)
public static ComponentAssembly.SubstitutionMode[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.