public static class Component.RepresentationMode extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXACT
The component's solid bodies are displayed with the exact data
|
static int |
_LIGHTWEIGHT
The component's solid bodies are all displayed using the lightweight representation
|
static int |
_NONE
There are no bodies to display for the current component
|
static int |
_PARTIAL
The component's solid bodies are displayed with some being exact and some being shown lightweight
|
static Component.RepresentationMode |
EXACT
The component's solid bodies are displayed with the exact data
|
static Component.RepresentationMode |
LIGHTWEIGHT
The component's solid bodies are all displayed using the lightweight representation
|
static Component.RepresentationMode |
NONE
There are no bodies to display for the current component
|
static Component.RepresentationMode |
PARTIAL
The component's solid bodies are displayed with some being exact and some being shown lightweight
|
Modifier and Type | Method and Description |
---|---|
static Component.RepresentationMode |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Component.RepresentationMode |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Component.RepresentationMode[] |
values()
Returns an array that contains the values for this enum.
|
public static final Component.RepresentationMode LIGHTWEIGHT
public static final Component.RepresentationMode PARTIAL
public static final Component.RepresentationMode EXACT
public static final Component.RepresentationMode NONE
public static final int _LIGHTWEIGHT
public static final int _PARTIAL
public static final int _EXACT
public static final int _NONE
public static Component.RepresentationMode valueOf(int value)
public static Component.RepresentationMode valueOf(String name)
public static Component.RepresentationMode[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.