public static class AssembliesGeneralPropertiesBuilder.HiddenOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MIXED
Objects hidden properties differ and will not change
|
static int |
_NO
Do not hide the objects
|
static int |
_YES
Hide the objects
|
static AssembliesGeneralPropertiesBuilder.HiddenOptions |
MIXED
Objects hidden properties differ and will not change
|
static AssembliesGeneralPropertiesBuilder.HiddenOptions |
NO
Do not hide the objects
|
static AssembliesGeneralPropertiesBuilder.HiddenOptions |
YES
Hide the objects
|
Modifier and Type | Method and Description |
---|---|
static AssembliesGeneralPropertiesBuilder.HiddenOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssembliesGeneralPropertiesBuilder.HiddenOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssembliesGeneralPropertiesBuilder.HiddenOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final AssembliesGeneralPropertiesBuilder.HiddenOptions NO
public static final AssembliesGeneralPropertiesBuilder.HiddenOptions YES
public static final AssembliesGeneralPropertiesBuilder.HiddenOptions MIXED
public static final int _NO
public static final int _YES
public static final int _MIXED
public static AssembliesGeneralPropertiesBuilder.HiddenOptions valueOf(int value)
public static AssembliesGeneralPropertiesBuilder.HiddenOptions valueOf(String name)
public static AssembliesGeneralPropertiesBuilder.HiddenOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.