Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static AssociativityLineOption |
AssociativityLineOption.ANGLE
At angle
|
static AssociativityLineOption |
AssociativityLineOption.BASE_LINE
Base line
|
static AssociativityLineOption |
AssociativityLineOption.CENTERLINE
Centerline -
Linear Bolt circle Circular |
static AssociativityLineOption |
AssociativityLineOption.EXISTING_LINE
Existing line
|
static AssociativityLineOption |
AssociativityLineOption.EXTENSION_LINE
Extension line
|
static AssociativityLineOption |
AssociativityLineOption.HORIZONTAL_LEFT
Horizontal left
|
static AssociativityLineOption |
AssociativityLineOption.HORIZONTAL_RIGHT
Horizontal right
|
static AssociativityLineOption |
AssociativityLineOption.LAST
Last enum value.
|
static AssociativityLineOption |
AssociativityLineOption.NONE
No line
|
static AssociativityLineOption |
AssociativityLineOption.POINT_VECTOR
Vector from two points
|
static AssociativityLineOption |
AssociativityLineOption.VERTICAL_DOWN
Vertical down
|
static AssociativityLineOption |
AssociativityLineOption.VERTICAL_UP
Vertical up
|
Modifier and Type | Method and Description |
---|---|
AssociativityLineOption |
AssociativityBuilder.lineOption()
Returns the line option
License requirements: None. |
AssociativityLineOption |
Associativity.lineOption()
Returns the line option
License requirements: None. |
static AssociativityLineOption |
AssociativityLineOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssociativityLineOption |
AssociativityLineOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssociativityLineOption[] |
AssociativityLineOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssociativityBuilder.setLineOption(AssociativityLineOption lineOption)
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
void |
Associativity.setLineOption(AssociativityLineOption lineOption)
Sets the line option
License requirements: None. |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.