public class ZeroToleranceDisplayStyle extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AS_ZERO
Always display zero tolerance as 0
|
static int |
_BASED_ON_UNITS
Zero tolerance display is tied to display units
|
static int |
_OMITTED
Omit the display of zero tolerance and maintain position of remaining tolerance
|
static int |
_OMITTED_AND_INLINED
Omit the display of zero tolerance and inline the remaining tolerance
|
static ZeroToleranceDisplayStyle |
AS_ZERO
Always display zero tolerance as 0
|
static ZeroToleranceDisplayStyle |
BASED_ON_UNITS
Zero tolerance display is tied to display units
|
static ZeroToleranceDisplayStyle |
OMITTED
Omit the display of zero tolerance and maintain position of remaining tolerance
|
static ZeroToleranceDisplayStyle |
OMITTED_AND_INLINED
Omit the display of zero tolerance and inline the remaining tolerance
|
Modifier and Type | Method and Description |
---|---|
static ZeroToleranceDisplayStyle |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ZeroToleranceDisplayStyle |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ZeroToleranceDisplayStyle[] |
values()
Returns an array that contains the values for this enum.
|
public static final ZeroToleranceDisplayStyle BASED_ON_UNITS
public static final ZeroToleranceDisplayStyle AS_ZERO
public static final ZeroToleranceDisplayStyle OMITTED_AND_INLINED
public static final ZeroToleranceDisplayStyle OMITTED
public static final int _BASED_ON_UNITS
public static final int _AS_ZERO
public static final int _OMITTED_AND_INLINED
public static final int _OMITTED
public static ZeroToleranceDisplayStyle valueOf(int value)
public static ZeroToleranceDisplayStyle valueOf(String name)
public static ZeroToleranceDisplayStyle[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.