public static class SymmetricalCenterlineBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FROM_FACE
Centerline from face
|
static int |
_START_AND_END
Centerline from start and end point
|
static SymmetricalCenterlineBuilder.Types |
FROM_FACE
Centerline from face
|
static SymmetricalCenterlineBuilder.Types |
START_AND_END
Centerline from start and end point
|
Modifier and Type | Method and Description |
---|---|
static SymmetricalCenterlineBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SymmetricalCenterlineBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SymmetricalCenterlineBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final SymmetricalCenterlineBuilder.Types FROM_FACE
public static final SymmetricalCenterlineBuilder.Types START_AND_END
public static final int _FROM_FACE
public static final int _START_AND_END
public static SymmetricalCenterlineBuilder.Types valueOf(int value)
public static SymmetricalCenterlineBuilder.Types valueOf(String name)
public static SymmetricalCenterlineBuilder.Types[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.