public static class IntersectionSymbolBuilder.Thickness extends Enum
Modifier and Type | Method and Description |
---|---|
static IntersectionSymbolBuilder.Thickness |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IntersectionSymbolBuilder.Thickness |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IntersectionSymbolBuilder.Thickness[] |
values()
Returns an array that contains the values for this enum.
|
public static final IntersectionSymbolBuilder.Thickness THIN
public static final IntersectionSymbolBuilder.Thickness NORMAL
public static final IntersectionSymbolBuilder.Thickness THICK
public static final IntersectionSymbolBuilder.Thickness ONE
public static final IntersectionSymbolBuilder.Thickness TWO
public static final IntersectionSymbolBuilder.Thickness THREE
public static final IntersectionSymbolBuilder.Thickness FOUR
public static final IntersectionSymbolBuilder.Thickness FIVE
public static final IntersectionSymbolBuilder.Thickness SIX
public static final IntersectionSymbolBuilder.Thickness SEVEN
public static final IntersectionSymbolBuilder.Thickness EIGHT
public static final IntersectionSymbolBuilder.Thickness NINE
public static final int _THIN
public static final int _NORMAL
public static final int _THICK
public static final int _ONE
public static final int _TWO
public static final int _THREE
public static final int _FOUR
public static final int _FIVE
public static final int _SIX
public static final int _SEVEN
public static final int _EIGHT
public static final int _NINE
public static IntersectionSymbolBuilder.Thickness valueOf(int value)
public static IntersectionSymbolBuilder.Thickness valueOf(String name)
public static IntersectionSymbolBuilder.Thickness[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.