public static class CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PARALLEL
The Plane of the PMI Cutting Plane Symbol Text is Parallel to its Arrow.
|
static int |
_PERPENDICULAR
The Plane of the PMI Cutting Plane Symbol Text is Perpendicular to its Arrow.
|
static CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow |
PARALLEL
The Plane of the PMI Cutting Plane Symbol Text is Parallel to its Arrow.
|
static CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow |
PERPENDICULAR
The Plane of the PMI Cutting Plane Symbol Text is Perpendicular to its Arrow.
|
Modifier and Type | Method and Description |
---|---|
static CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow[] |
values()
Returns an array that contains the values for this enum.
|
public static final CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow PARALLEL
public static final CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow PERPENDICULAR
public static final int _PARALLEL
public static final int _PERPENDICULAR
public static CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow valueOf(int value)
public static CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow valueOf(String name)
public static CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.