public interface CircleCenterlineBuilder extends CenterlineBuilder
Property | Value |
---|---|
Settings.Extension | 6.35 (millimeters part), 0.25 (inches part) |
Settings.Gap | 1.5875 (millimeters part), 0.0625 (inches part) |
Settings.IndividualDistance | 0 |
Settings.Size | 3.175 (millimeters part), 0.125 (inches part) |
Settings.Width | Thin |
Modifier and Type | Interface and Description |
---|---|
static class |
CircleCenterlineBuilder.Types
the valid enumeration used for the creation types, applicable only while creation
Once created type centerpoint will be set for all bolt circle/circular centerline
|
Modifier and Type | Method and Description |
---|---|
boolean |
fullCircle()
Returns the method which returns full or partial circle flag
License requirements: None. |
SelectNXObject |
inherit()
Returns the inherit object
License requirements: None. |
SelectNXObjectList |
locations()
Returns the selction object of the centerline
License requirements: None. |
void |
removeLocation(int index)
Removes location object for a given index from the Select Object List.
|
void |
setFullCircle(boolean fullType)
License requirements: drafting ("DRAFTING") . |
CircleCenterlineSettingsBuilder |
settings()
Returns the settings builder object for the centerline
License requirements: None. |
void |
setType(CircleCenterlineBuilder.Types method)
License requirements: drafting ("DRAFTING") . |
CircleCenterlineBuilder.Types |
type()
Returns the method which returns type of centerline
License requirements: None. |
addEndExtensions, addExtension, getAllExtensions, getAllIndividualExtensions, getEndExtensions, removeEndExtensions, removeExtension, resetAllExtensions, setAllIndividualExtensions, setEndExtensions, setIndividualExtensions
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectNXObjectList locations() throws NXException, RemoteException
NXException
RemoteException
boolean fullCircle() throws NXException, RemoteException
NXException
RemoteException
void setFullCircle(boolean fullType) throws NXException, RemoteException
fullType
- NXException
RemoteException
CircleCenterlineBuilder.Types type() throws NXException, RemoteException
NXException
RemoteException
void setType(CircleCenterlineBuilder.Types method) throws NXException, RemoteException
method
- NXException
RemoteException
SelectNXObject inherit() throws NXException, RemoteException
NXException
RemoteException
CircleCenterlineSettingsBuilder settings() throws NXException, RemoteException
NXException
RemoteException
void removeLocation(int index) throws NXException, RemoteException
index
- Index of the object in the select object listNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.