public class ChamferOrientationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HORIZONTAL
default (same as the adjacent edge)
|
static int |
_PARALLEL
parallel to the chamfer line itself
|
static int |
_VERTICAL
perpendicular with default
|
static ChamferOrientationType |
HORIZONTAL
default (same as the adjacent edge)
|
static ChamferOrientationType |
PARALLEL
parallel to the chamfer line itself
|
static ChamferOrientationType |
VERTICAL
perpendicular with default
|
Modifier and Type | Method and Description |
---|---|
static ChamferOrientationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ChamferOrientationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ChamferOrientationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ChamferOrientationType HORIZONTAL
public static final ChamferOrientationType VERTICAL
public static final ChamferOrientationType PARALLEL
public static final int _HORIZONTAL
public static final int _VERTICAL
public static final int _PARALLEL
public static ChamferOrientationType valueOf(int value)
public static ChamferOrientationType valueOf(String name)
public static ChamferOrientationType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.