public static class Update.Option extends Enum
Update.doUpdate(int)
at a
later time. Some methods in the Common API may perform an update. In an effort to
improve performance, these methods take an option as input to not perform an update.
For example, a method called in a loop may set the option to not update and then perform
an explicit update after the loop completes.
Modifier and Type | Field and Description |
---|---|
static int |
_LATER
Do not perform an update
|
static int |
_NOW
Perform an update immediately
|
static Update.Option |
LATER
Do not perform an update
|
static Update.Option |
NOW
Perform an update immediately
|
Modifier and Type | Method and Description |
---|---|
static Update.Option |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Update.Option |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Update.Option[] |
values()
Returns an array that contains the values for this enum.
|
public static final Update.Option NOW
public static final Update.Option LATER
public static final int _NOW
public static final int _LATER
public static Update.Option valueOf(int value)
public static Update.Option valueOf(String name)
public static Update.Option[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.