public static class SketchAlongPathBuilder.SketchOrientationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC
Automatic
|
static int |
_RELATIVE_TO_FACE
Relative to face
|
static int |
_USE_CURVE_PARAMETERS
Based on curve parameter
|
static SketchAlongPathBuilder.SketchOrientationType |
AUTOMATIC
Automatic
|
static SketchAlongPathBuilder.SketchOrientationType |
RELATIVE_TO_FACE
Relative to face
|
static SketchAlongPathBuilder.SketchOrientationType |
USE_CURVE_PARAMETERS
Based on curve parameter
|
Modifier and Type | Method and Description |
---|---|
static SketchAlongPathBuilder.SketchOrientationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchAlongPathBuilder.SketchOrientationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchAlongPathBuilder.SketchOrientationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SketchAlongPathBuilder.SketchOrientationType AUTOMATIC
public static final SketchAlongPathBuilder.SketchOrientationType RELATIVE_TO_FACE
public static final SketchAlongPathBuilder.SketchOrientationType USE_CURVE_PARAMETERS
public static final int _AUTOMATIC
public static final int _RELATIVE_TO_FACE
public static final int _USE_CURVE_PARAMETERS
public static SketchAlongPathBuilder.SketchOrientationType valueOf(int value)
public static SketchAlongPathBuilder.SketchOrientationType valueOf(String name)
public static SketchAlongPathBuilder.SketchOrientationType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.