public static class SketchAlignmentConstraint.Type extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HORIZONTAL
The two vertices are horizontally aligned
|
static int |
_VERTICAL
The two vertices are vertically aligned
|
static SketchAlignmentConstraint.Type |
HORIZONTAL
The two vertices are horizontally aligned
|
static SketchAlignmentConstraint.Type |
VERTICAL
The two vertices are vertically aligned
|
Modifier and Type | Method and Description |
---|---|
static SketchAlignmentConstraint.Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchAlignmentConstraint.Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchAlignmentConstraint.Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final SketchAlignmentConstraint.Type HORIZONTAL
public static final SketchAlignmentConstraint.Type VERTICAL
public static final int _HORIZONTAL
public static final int _VERTICAL
public static SketchAlignmentConstraint.Type valueOf(int value)
public static SketchAlignmentConstraint.Type valueOf(String name)
public static SketchAlignmentConstraint.Type[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.