public static class Sketch.AutoDimensioningRule extends Enum
SYMMETRIC
: create symmetric dimensions if the curves are symmetric
ADJACENT_ANGLE
: create angles between adjacent lines
LENGTH
: create length dimension for lines
HORIZONTAL_VERTICAL
: create horizontal and vertical dimensions
REFERENCE_AXES
: create dimensions between curves and reference axesModifier and Type | Field and Description |
---|---|
static int |
_ADJACENT_ANGLE
Create Adjacent Angles
|
static int |
_HORIZONTAL_VERTICAL
Create Horizontal and Vertical Dimensions
|
static int |
_LENGTH
Create Length Dimension
|
static int |
_REFERENCE_AXES
Create Dimensions to Reference Axes
|
static int |
_SYMMETRIC
Create Symmetric Dimensions
|
static Sketch.AutoDimensioningRule |
ADJACENT_ANGLE
Create Adjacent Angles
|
static Sketch.AutoDimensioningRule |
HORIZONTAL_VERTICAL
Create Horizontal and Vertical Dimensions
|
static Sketch.AutoDimensioningRule |
LENGTH
Create Length Dimension
|
static Sketch.AutoDimensioningRule |
REFERENCE_AXES
Create Dimensions to Reference Axes
|
static Sketch.AutoDimensioningRule |
SYMMETRIC
Create Symmetric Dimensions
|
Modifier and Type | Method and Description |
---|---|
static Sketch.AutoDimensioningRule |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.AutoDimensioningRule |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.AutoDimensioningRule[] |
values()
Returns an array that contains the values for this enum.
|
public static final Sketch.AutoDimensioningRule SYMMETRIC
public static final Sketch.AutoDimensioningRule ADJACENT_ANGLE
public static final Sketch.AutoDimensioningRule LENGTH
public static final Sketch.AutoDimensioningRule HORIZONTAL_VERTICAL
public static final Sketch.AutoDimensioningRule REFERENCE_AXES
public static final int _SYMMETRIC
public static final int _ADJACENT_ANGLE
public static final int _LENGTH
public static final int _HORIZONTAL_VERTICAL
public static final int _REFERENCE_AXES
public static Sketch.AutoDimensioningRule valueOf(int value)
public static Sketch.AutoDimensioningRule valueOf(String name)
public static Sketch.AutoDimensioningRule[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.