public static class PropertyContainer.ListMode extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INDEXED
The properties are not named and
must be indexed through an integer index
|
static int |
_NAMED
The properties are named
|
static PropertyContainer.ListMode |
INDEXED
The properties are not named and
must be indexed through an integer index
|
static PropertyContainer.ListMode |
NAMED
The properties are named
|
Modifier and Type | Method and Description |
---|---|
static PropertyContainer.ListMode |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PropertyContainer.ListMode |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PropertyContainer.ListMode[] |
values()
Returns an array that contains the values for this enum.
|
public static final PropertyContainer.ListMode INDEXED
public static final PropertyContainer.ListMode NAMED
public static final int _INDEXED
public static final int _NAMED
public static PropertyContainer.ListMode valueOf(int value)
public static PropertyContainer.ListMode valueOf(String name)
public static PropertyContainer.ListMode[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.