public static class PlotBuilder.RotationOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEGREE0
0 degree rotation
|
static int |
_DEGREE180
180 degree rotation
|
static int |
_DEGREE270
270 degree rotation
|
static int |
_DEGREE90
90 degree rotation
|
static PlotBuilder.RotationOption |
DEGREE0
0 degree rotation
|
static PlotBuilder.RotationOption |
DEGREE180
180 degree rotation
|
static PlotBuilder.RotationOption |
DEGREE270
270 degree rotation
|
static PlotBuilder.RotationOption |
DEGREE90
90 degree rotation
|
Modifier and Type | Method and Description |
---|---|
static PlotBuilder.RotationOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlotBuilder.RotationOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlotBuilder.RotationOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final PlotBuilder.RotationOption DEGREE0
public static final PlotBuilder.RotationOption DEGREE90
public static final PlotBuilder.RotationOption DEGREE180
public static final PlotBuilder.RotationOption DEGREE270
public static final int _DEGREE0
public static final int _DEGREE90
public static final int _DEGREE180
public static final int _DEGREE270
public static PlotBuilder.RotationOption valueOf(int value)
public static PlotBuilder.RotationOption valueOf(String name)
public static PlotBuilder.RotationOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.