public static class PartCollection.WorkComponentOption extends Enum
PartCollection.setWorkComponent(nxopen.assemblies.Component)
Modifier and Type | Field and Description |
---|---|
static int |
_GIVEN
Use the given work component, regardless of visibility.
|
static int |
_VISIBLE
If the given work component is not visible, chose another component that
represents the same part.
|
static PartCollection.WorkComponentOption |
GIVEN
Use the given work component, regardless of visibility.
|
static PartCollection.WorkComponentOption |
VISIBLE
If the given work component is not visible, chose another component that
represents the same part.
|
Modifier and Type | Method and Description |
---|---|
static PartCollection.WorkComponentOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartCollection.WorkComponentOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartCollection.WorkComponentOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartCollection.WorkComponentOption VISIBLE
public static final PartCollection.WorkComponentOption GIVEN
public static final int _VISIBLE
public static final int _GIVEN
public static PartCollection.WorkComponentOption valueOf(int value)
public static PartCollection.WorkComponentOption valueOf(String name)
public static PartCollection.WorkComponentOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.