public interface MaterialUtilities extends Remote
MaterialUtilities
class CaeSession
Modifier and Type | Interface and Description |
---|---|
static class |
MaterialUtilities.ConvertStressStrainData
This class holds the data returned from
convertStressStrainData(double[], double[], double, double, nxopen.MaterialUtilities.StressStrainData, nxopen.MaterialUtilities.StressStrainData) |
static class |
MaterialUtilities.ConvertStressStrainYoungsModulusData
This class holds the data returned from
convertStressStrainYoungsModulusData(double[], double[], double, double, nxopen.MaterialUtilities.StressStrainData, nxopen.MaterialUtilities.StressStrainData) |
static class |
MaterialUtilities.StressStrainData
The stress strain data type
|
Modifier and Type | Method and Description |
---|---|
MaterialUtilities.ConvertStressStrainData |
convertStressStrainData(double[] strainData,
double[] stressData,
double youngsModulus,
double poissionRatio,
MaterialUtilities.StressStrainData inputDataType,
MaterialUtilities.StressStrainData outputDataType)
Deprecated.
|
MaterialUtilities.ConvertStressStrainYoungsModulusData |
convertStressStrainYoungsModulusData(double[] strainData,
double[] stressData,
double youngsModulus,
double poissionRatio,
MaterialUtilities.StressStrainData inputDataType,
MaterialUtilities.StressStrainData outputDataType)
Convert stress strain data between the four types EngineeringStressEngineeringStrain,
EngineeringStressEngineeringPlasticStrain, TrueStressLogStrain and TrueStressLogPlasticStrain.
|
MaterialUtilities.ConvertStressStrainData convertStressStrainData(double[] strainData, double[] stressData, double youngsModulus, double poissionRatio, MaterialUtilities.StressStrainData inputDataType, MaterialUtilities.StressStrainData outputDataType) throws NXException, RemoteException
convertStressStrainYoungsModulusData(double[], double[], double, double, nxopen.MaterialUtilities.StressStrainData, nxopen.MaterialUtilities.StressStrainData)
instead.
strainData
- the input strain arraystressData
- the input stress arrayyoungsModulus
- the input young's modulus used in converting algorithmpoissionRatio
- the input poission's ratio used in converting algorithminputDataType
- the input stress-strain data typeoutputDataType
- the output stress-strain data type
NXException
RemoteException
MaterialUtilities.ConvertStressStrainYoungsModulusData convertStressStrainYoungsModulusData(double[] strainData, double[] stressData, double youngsModulus, double poissionRatio, MaterialUtilities.StressStrainData inputDataType, MaterialUtilities.StressStrainData outputDataType) throws NXException, RemoteException
strainData
- the input strain arraystressData
- the input stress arrayyoungsModulus
- the input young's modulus used in converting algorithmpoissionRatio
- the input poission's ratio used in converting algorithminputDataType
- the input stress-strain data typeoutputDataType
- the output stress-strain data typeNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.