public class LightType extends Enum
SCENE
via automation languages.
Modifier and Type | Field and Description |
---|---|
static int |
_AMBIENT
An ambient light provides global illumination
for the scene.
|
static int |
_DISTANT
A distant light can be thought of as being
located for all practical purposes infinitely far away,
such as the sun.
|
static int |
_EYE
An eye light is Located at the viewpoint or directly
on the Z axis of the screen.
|
static int |
_POINT
A point light emits light equally in all directions.
|
static int |
_SCENE
A scene lights is a light whose parameters, except for
intensity, are fixed.
|
static int |
_SPOT
A spot light is the same as a point light,
except that it is constrained by a cone shape.
|
static LightType |
AMBIENT
An ambient light provides global illumination
for the scene.
|
static LightType |
DISTANT
A distant light can be thought of as being
located for all practical purposes infinitely far away,
such as the sun.
|
static LightType |
EYE
An eye light is Located at the viewpoint or directly
on the Z axis of the screen.
|
static LightType |
POINT
A point light emits light equally in all directions.
|
static LightType |
SCENE
A scene lights is a light whose parameters, except for
intensity, are fixed.
|
static LightType |
SPOT
A spot light is the same as a point light,
except that it is constrained by a cone shape.
|
Modifier and Type | Method and Description |
---|---|
static LightType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LightType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LightType[] |
values()
Returns an array that contains the values for this enum.
|
public static final LightType AMBIENT
public static final LightType DISTANT
public static final LightType EYE
public static final LightType POINT
public static final LightType SPOT
public static final LightType SCENE
public static final int _AMBIENT
public static final int _DISTANT
public static final int _EYE
public static final int _POINT
public static final int _SPOT
public static final int _SCENE
public static LightType valueOf(int value)
public static LightType valueOf(String name)
public static LightType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.