public interface ISketchHelpedConstraint extends INXObject
Modifier and Type | Interface and Description |
---|---|
static class |
ISketchHelpedConstraint.HelpData
This class holds the data returned from
getHelpData() |
Modifier and Type | Method and Description |
---|---|
ISketchHelpedConstraint.HelpData |
getHelpData()
Gets the help data for the constraint
License requirements: None. |
void |
setHelpParameters(boolean hasHelp1,
boolean hasHelp2,
double helpParameter1,
double helpParameter2)
Sets the help parameters for the constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
void |
setHelpPoints(boolean hasHelp1,
boolean hasHelp2,
Point3d helpPoint1,
Point3d helpPoint2)
Sets the help points for the constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
ISketchHelpedConstraint.HelpData getHelpData() throws NXException, RemoteException
NXException
RemoteException
void setHelpPoints(boolean hasHelp1, boolean hasHelp2, Point3d helpPoint1, Point3d helpPoint2) throws NXException, RemoteException
hasHelp1
- Whether the constraint's first associated geometric item has an associated help pointhasHelp2
- Whether the constraint's second associated geometric item has an associated help pointhelpPoint1
- The first help point. Not used unless has_help1 is true.helpPoint2
- The second help point. Not used unless has_help2 is true.NXException
RemoteException
void setHelpParameters(boolean hasHelp1, boolean hasHelp2, double helpParameter1, double helpParameter2) throws NXException, RemoteException
hasHelp1
- Whether the constraint's first associated geometric item has an associated help parameterhasHelp2
- Whether the constraint's second associated geometric item has an associated help parameterhelpParameter1
- The first help parameter. Not used unless has_help1 is true.helpParameter2
- The second help parameter. Not used unless has_help2 is true.NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.