public static class GenericMeasure.Type extends Enum
Modifier and Type | Method and Description |
---|---|
static GenericMeasure.Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GenericMeasure.Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GenericMeasure.Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final GenericMeasure.Type MINIMUM_DISTANCE
public static final GenericMeasure.Type LOCAL_MINIMUM_DISTANCE
public static final GenericMeasure.Type MAXIMUM_DISTANCE
public static final GenericMeasure.Type PROJECTED_DISTANCE
public static final GenericMeasure.Type RADIAL_DISTANCE
public static final GenericMeasure.Type LENGTH
public static final GenericMeasure.Type TWO_OBJECT_ANGLE
public static final GenericMeasure.Type THREE_POINT_ANGLE
public static final GenericMeasure.Type FACE_PROPERTIES
public static final GenericMeasure.Type MASS_PROPERTIES
public static final GenericMeasure.Type POINTS_ON_CURVES
public static final GenericMeasure.Type ROUTING_PATH_LENGTH
public static final GenericMeasure.Type DIAMETER_DISTANCE
public static final GenericMeasure.Type POLAR_RADIUS
public static final GenericMeasure.Type POLAR_ANGLE
public static final GenericMeasure.Type RECTANGULAR_EXTREME
public static final GenericMeasure.Type POLAR_AREA
public static final GenericMeasure.Type MINIMUM_SMART_DISTANCE
public static final GenericMeasure.Type MAXIMUM_SMART_DISTANCE
public static final GenericMeasure.Type POINT
public static final int _MINIMUM_DISTANCE
public static final int _LOCAL_MINIMUM_DISTANCE
public static final int _MAXIMUM_DISTANCE
public static final int _PROJECTED_DISTANCE
public static final int _RADIAL_DISTANCE
public static final int _LENGTH
public static final int _TWO_OBJECT_ANGLE
public static final int _THREE_POINT_ANGLE
public static final int _FACE_PROPERTIES
public static final int _MASS_PROPERTIES
public static final int _POINTS_ON_CURVES
public static final int _ROUTING_PATH_LENGTH
public static final int _DIAMETER_DISTANCE
public static final int _POLAR_RADIUS
public static final int _POLAR_ANGLE
public static final int _RECTANGULAR_EXTREME
public static final int _POLAR_AREA
public static final int _MINIMUM_SMART_DISTANCE
public static final int _MAXIMUM_SMART_DISTANCE
public static final int _POINT
public static GenericMeasure.Type valueOf(int value)
public static GenericMeasure.Type valueOf(String name)
public static GenericMeasure.Type[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.