public static class DisplayManager.FacetCacheMemoryLevelType extends Enum
DisplayManager.facetCacheMemoryLevel()
and DisplayManager.setFacetCacheMemoryLevel(nxopen.DisplayManager.FacetCacheMemoryLevelType)
Modifier and Type | Field and Description |
---|---|
static int |
_NONE |
static int |
_ONE |
static int |
_THREE |
static int |
_TWO |
static DisplayManager.FacetCacheMemoryLevelType |
NONE |
static DisplayManager.FacetCacheMemoryLevelType |
ONE |
static DisplayManager.FacetCacheMemoryLevelType |
THREE |
static DisplayManager.FacetCacheMemoryLevelType |
TWO |
Modifier and Type | Method and Description |
---|---|
static DisplayManager.FacetCacheMemoryLevelType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DisplayManager.FacetCacheMemoryLevelType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DisplayManager.FacetCacheMemoryLevelType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DisplayManager.FacetCacheMemoryLevelType NONE
public static final DisplayManager.FacetCacheMemoryLevelType ONE
public static final DisplayManager.FacetCacheMemoryLevelType TWO
public static final DisplayManager.FacetCacheMemoryLevelType THREE
public static final int _NONE
public static final int _ONE
public static final int _TWO
public static final int _THREE
public static DisplayManager.FacetCacheMemoryLevelType valueOf(int value)
public static DisplayManager.FacetCacheMemoryLevelType valueOf(String name)
public static DisplayManager.FacetCacheMemoryLevelType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.