public static class DatumConstraint.Solution extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BINORMAL |
static int |
_NORMAL |
static int |
_OPPOSITE_BINORMAL
Datum axis at opposite to binormal to curve
|
static int |
_OPPOSITE_NORMAL |
static int |
_OPPOSITE_TANGENT |
static int |
_PROJECT
This direction is calculated by projecting a point selected along a curve
to a line, a datum axis, an edge of a solid, a planar face or a datum plane
|
static int |
_TANGENT |
static int |
_UNDEFINED |
static DatumConstraint.Solution |
BINORMAL |
static DatumConstraint.Solution |
NORMAL |
static DatumConstraint.Solution |
OPPOSITE_BINORMAL
Datum axis at opposite to binormal to curve
|
static DatumConstraint.Solution |
OPPOSITE_NORMAL |
static DatumConstraint.Solution |
OPPOSITE_TANGENT |
static DatumConstraint.Solution |
PROJECT
This direction is calculated by projecting a point selected along a curve
to a line, a datum axis, an edge of a solid, a planar face or a datum plane
|
static DatumConstraint.Solution |
TANGENT |
static DatumConstraint.Solution |
UNDEFINED |
Modifier and Type | Method and Description |
---|---|
static DatumConstraint.Solution |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumConstraint.Solution |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumConstraint.Solution[] |
values()
Returns an array that contains the values for this enum.
|
public static final DatumConstraint.Solution UNDEFINED
public static final DatumConstraint.Solution TANGENT
public static final DatumConstraint.Solution NORMAL
public static final DatumConstraint.Solution BINORMAL
public static final DatumConstraint.Solution OPPOSITE_TANGENT
public static final DatumConstraint.Solution OPPOSITE_NORMAL
public static final DatumConstraint.Solution OPPOSITE_BINORMAL
public static final DatumConstraint.Solution PROJECT
public static final int _UNDEFINED
public static final int _TANGENT
public static final int _NORMAL
public static final int _BINORMAL
public static final int _OPPOSITE_TANGENT
public static final int _OPPOSITE_NORMAL
public static final int _OPPOSITE_BINORMAL
public static final int _PROJECT
public static DatumConstraint.Solution valueOf(int value)
public static DatumConstraint.Solution valueOf(String name)
public static DatumConstraint.Solution[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.