public static class CaeObjectType.CaeSubType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ELEMENT_EDGE
sub type is element edge
|
static int |
_ELEMENT_FACE
sub type is element face
|
static int |
_NONE
sub type is the same as the type of the object
|
static CaeObjectType.CaeSubType |
ELEMENT_EDGE
sub type is element edge
|
static CaeObjectType.CaeSubType |
ELEMENT_FACE
sub type is element face
|
static CaeObjectType.CaeSubType |
NONE
sub type is the same as the type of the object
|
Modifier and Type | Method and Description |
---|---|
static CaeObjectType.CaeSubType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CaeObjectType.CaeSubType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CaeObjectType.CaeSubType[] |
values()
Returns an array that contains the values for this enum.
|
public static final CaeObjectType.CaeSubType NONE
public static final CaeObjectType.CaeSubType ELEMENT_FACE
public static final CaeObjectType.CaeSubType ELEMENT_EDGE
public static final int _NONE
public static final int _ELEMENT_FACE
public static final int _ELEMENT_EDGE
public static CaeObjectType.CaeSubType valueOf(int value)
public static CaeObjectType.CaeSubType valueOf(String name)
public static CaeObjectType.CaeSubType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.