public static class AutomaticTraceline.ModeOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EVALUATE
Evaluate which mode to use
|
static int |
_INFER
Infer orientation from start and end directions
|
static int |
_ORIENTATION
Align with orientation
|
static AutomaticTraceline.ModeOption |
EVALUATE
Evaluate which mode to use
|
static AutomaticTraceline.ModeOption |
INFER
Infer orientation from start and end directions
|
static AutomaticTraceline.ModeOption |
ORIENTATION
Align with orientation
|
Modifier and Type | Method and Description |
---|---|
static AutomaticTraceline.ModeOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AutomaticTraceline.ModeOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AutomaticTraceline.ModeOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final AutomaticTraceline.ModeOption EVALUATE
public static final AutomaticTraceline.ModeOption ORIENTATION
public static final AutomaticTraceline.ModeOption INFER
public static final int _EVALUATE
public static final int _ORIENTATION
public static final int _INFER
public static AutomaticTraceline.ModeOption valueOf(int value)
public static AutomaticTraceline.ModeOption valueOf(String name)
public static AutomaticTraceline.ModeOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.