UserDefinedObjectManager Class

class NXOpen.UserDefinedObjects.UserDefinedObjectManager

Bases: object

This class creates and manages UserDefinedObjects

To obtain an instance of this class, refer to NXOpen.BasePart

New in version NX5.0.0.

Methods

Method Description
CreateUserDefinedObject Constructs a new NXOpen.Features.UserDefinedObjectFeature.
GetLinksToObject Queries an NX Object to find all UserDefinedObjects.UserDefinedObject‘s that are linked to the given NXObject (note this will not find owning udos) @return The link definitions from UDO’s to the NXObject
GetOwningUserDefinedObject Queries an NX Object to find the UserDefinedObjects.UserDefinedObject that owns the given NXObject (note this will return null for the owning udo if the object is not owned) @return The UDO which owns the NXObject
GetUdosOfClass Finds all UserDefinedObjects.UserDefinedObject instances that use the given NXOpen.UserDefinedObjects.UserDefinedClass.
IsObjectLinkable Queries an NX Object to see if it can be linked to a UserDefinedObjects.UserDefinedObject via the given link type @return TRUE - This object can be linked to a UDO with the given link type, FALSE - this object can not be NOT linked to a UDO with the given link type
IsObjectLinkedToUserDefinedObject Queries an NX Object to see if it is linked to a UserDefinedObjects.UserDefinedObject (note this will not tell you if the object is owned by a UDO with an owning link) @return TRUE - This object is linked to a UDO, FALSE - this object is NOT linked to a UDO
IsObjectOwnedByUserDefinedObject Queries an NX Object to see if it is owned by a UserDefinedObjects.UserDefinedObject @return TRUE - This object is owned by a UDO, FALSE - this object is NOT owned by a UDO

Structs

UserDefinedObjectManagerLinkedUdoDefinition_Struct Struct Used to define a link to a UserDefinedObject

Method Detail

CreateUserDefinedObject

UserDefinedObjectManager.CreateUserDefinedObject

Constructs a new NXOpen.Features.UserDefinedObjectFeature.

Signature CreateUserDefinedObject(udoClass)

Parameters:udoClass (NXOpen.UserDefinedObjects.UserDefinedClass) – The UserDefinedClass used to define the new UserDefinedObject
Returns:The new UserDefinedObject instance
Return type:NXOpen.UserDefinedObjects.UserDefinedObject

New in version NX5.0.0.

License requirements: None.

GetLinksToObject

UserDefinedObjectManager.GetLinksToObject

Queries an NX Object to find all UserDefinedObjects.UserDefinedObject‘s that are linked to the given NXObject (note this will not find owning udos)

Signature GetLinksToObject(linkObject)

Parameters:linkObject (NXOpen.TaggedObject) – NXObject to query for links
Returns:The link definitions from UDO’s to the NXObject
Return type:list of NXOpen.UserDefinedObjects.UserDefinedObjectManagerLinkedUdoDefinition_Struct

New in version NX5.0.0.

License requirements: None.

GetOwningUserDefinedObject

UserDefinedObjectManager.GetOwningUserDefinedObject

Queries an NX Object to find the UserDefinedObjects.UserDefinedObject that owns the given NXObject (note this will return null for the owning udo if the object is not owned)

Signature GetOwningUserDefinedObject(linkObject)

Parameters:linkObject (NXOpen.TaggedObject) – NXObject to query for an owning UDO
Returns:The UDO which owns the NXObject
Return type:NXOpen.UserDefinedObjects.UserDefinedObject

New in version NX5.0.0.

License requirements: None.

GetUdosOfClass

UserDefinedObjectManager.GetUdosOfClass

Finds all UserDefinedObjects.UserDefinedObject instances that use the given NXOpen.UserDefinedObjects.UserDefinedClass.

Signature GetUdosOfClass(udoClass)

Parameters:udoClass (NXOpen.UserDefinedObjects.UserDefinedClass) – The UserDefinedClass we want to find
Returns:User Defined Objects of the given class
Return type:list of NXOpen.UserDefinedObjects.UserDefinedObject

New in version NX5.0.0.

License requirements: None.

IsObjectLinkable

UserDefinedObjectManager.IsObjectLinkable

Queries an NX Object to see if it can be linked to a UserDefinedObjects.UserDefinedObject via the given link type

Signature IsObjectLinkable(linkObject, linkType)

Parameters:
Returns:

TRUE - This object can be linked to a UDO with the given link type, FALSE - this object can not be NOT linked to a UDO with the given link type

Return type:

bool

New in version NX5.0.0.

License requirements: None.

IsObjectLinkedToUserDefinedObject

UserDefinedObjectManager.IsObjectLinkedToUserDefinedObject

Queries an NX Object to see if it is linked to a UserDefinedObjects.UserDefinedObject (note this will not tell you if the object is owned by a UDO with an owning link)

Signature IsObjectLinkedToUserDefinedObject(linkObject)

Parameters:linkObject (NXOpen.TaggedObject) – NXObject to query for links
Returns:TRUE - This object is linked to a UDO, FALSE - this object is NOT linked to a UDO
Return type:bool

New in version NX5.0.0.

License requirements: None.

IsObjectOwnedByUserDefinedObject

UserDefinedObjectManager.IsObjectOwnedByUserDefinedObject

Queries an NX Object to see if it is owned by a UserDefinedObjects.UserDefinedObject

Signature IsObjectOwnedByUserDefinedObject(linkObject)

Parameters:linkObject (NXOpen.TaggedObject) – NXObject to query for an owning UDO
Returns:TRUE - This object is owned by a UDO, FALSE - this object is NOT owned by a UDO
Return type:bool

New in version NX5.0.0.

License requirements: None.